Posted on May 14, 2015 at 21:16How can i calculate the phase currents (ia, ib, ic) from the currents of the 3 shunt resistors placed under the lower switches of the inverter?like in steval-ihm023v3 #steval-ihm023v2
Posted on April 15, 2015 at 14:00pin 1 in the L6390 driver is LIN- (active low) Is this mean that the pulses of this input will be inverted ?also the pin SD-
Posted on March 18, 2015 at 20:30i ask about the board steval-ihm023v3 can i use any controller to drive it like DSP or arduino or i must use a special controller from ST ?also i didn't understand why we connect encoder ABZ signals to the board (we ...
Posted on April 15, 2015 at 13:49through j1 because it is the only jumper for supply also there is no problem when connecting DC voltage to rectifier J6 is for braking only