cancel
Showing results for 
Search instead for 
Did you mean: 

L6390 Driver IC question

shady_mamdouh_2011
Associate II
Posted on April 15, 2015 at 14:00

pin 1 in the L6390 driver is LIN- (active low) 

Is this mean that the pulses of this input will be inverted ?

also the pin SD-
This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Enrico Poli
ST Employee
Posted on April 27, 2015 at 09:04

Hi,

active low means that the respective function is activated when the logic signal is low instead of high (internally inverted).

e.g. forcing the SD pin low the device is shutdown.

Regards

Enrico