User Activity

Hello,My TouchGFX application (without an operating system) receives events from a communication channel, and in some cases, there are icons on the screen that need to change visibility based on the received state. The events are acquired during the ...
Hello!The CircleProgress and Circle widgets do not work with images on STM32H7 with a 1280x800 24bpp TFT (double buffered graphic mode), while they work correctly in the simulator.Circle widget:if under "Image & Color" I choose Color, it works on bot...
I'm trying to minimize the current consumption of an STM32G031K but I can't reach the ones calculated by the STM32CubeMX in any way. I tried with Low Power Sleep Mode, Stop Mode 0 and Stop mode 1. In Stop Mode 1, according to STM32CubeMX I should hav...
Kudos from