User Activity

Posted on October 27, 2014 at 00:34I am trying to get a USB CDC Device demo working on an STM32F4 Discovery board (with the STM32F407) with code from the STM32CubeMX generator application. The process has been murky at best, hopefully one of you can...
Posted on August 30, 2014 at 00:53I am attempting to communicate via I2C to another ST device (LPS331AP) and read its sensor values. However, I am not able to initiate the I2C session properly. On the wire, I can see that the start signal is actuall...
Posted on August 27, 2014 at 23:37Is there any reason why I could not (or you recommend to not) short the Vcc (pin 1&2) and Vdd (pin 19) lines on the ST-Link/V2 programmer during development? I would prefer to power the target application board, via...