User Activity

Question 1: are there any benefits to using standalone PD controller like STSUB1600 over integrated solution STM32G0x1Question 2: are there code examples that are reasonably close to the DRP functionality ? In all the X-CUBE-USB-PD examples I've see...
The errata suggest to "insert a dummy phase with at least two dummy cycles" when using indirect data read mode.However, according to the documentation of the dummy cycle phase (AN4760 rev 3, section 3.1.4 and figure 8 ) states that in the dummy phase...
Kudos from