2021-02-10 5:28 AM
Question 1: are there any benefits to using standalone PD controller like STSUB1600 over integrated solution STM32G0x1
Question 2: are there code examples that are reasonably close to the DRP functionality ? In all the X-CUBE-USB-PD examples I've seen it's very hard to follow the logic through all the boilerplate code, and not clear when is required to simply initialize the port.
2021-02-10 7:11 AM
Hello
DRP can connect as source or sink, depending on its counterpart.
It seems that your application needs is what is called 'sourcing device': power role is source while data role is UFP.
Depending on connection power role, application needs to do power or data role swap.
In our stusb1602 software package, we are proposing such project.
Hope it will fit your needs :)
Best regards
Nathalie
2021-02-17 9:11 AM
Hello,
you can also have a look at this wiki page.
Such power role swap application is available on STM32G0 and STM32G4 Evaluation boards.
The simplest software example will be available soon (end Q2) on a TCPP03 shield (for DRP), the equivalent of the already available TCPP01 shield (for Sink).
2021-02-17 2:03 PM
Thanks for the information. So I'll try to summarize what I learned - would appreciate corrections for any mistakes :
So since waiting 4 months is not really an option for us, the practical approach would seem to be using the USB reference design and code from the Nucleo-usb002 , and then trying to port the example to a processor with better availability (probably from G0x1 line) Does that make sense? Would example code be easily portable to different CPU?
2021-02-17 10:58 PM
Hello
STUSB1602 has currently FW package with stm32F072 - stm32F446 and stm32G474: available on web
We will have soon STM32L4R5 and stm32H723 (not available yet on web but available on demand)
If you have an other preferred stm32 we can have help you for the porting.
Best regards
Nathalie
2021-03-26 12:15 PM
Another quick question regarding USB002 (MB1303) board: which firmware and compilation switches are loaded there out of the box?
Is that _DRP_2PORTS project?
This is the output I am getting :
>p 0
DRP role Unplugged
Local Source PDOs:
1) 5.00V 1.50A
2) 9.00V 2.00A
3) 12.00V 2.00A
4) 20.00V 2.00A
Local Sink PDOs:
1) 5.00V 3.00A
> and yet GPIO_FOR_SRC seems to be disabled by default - so why am I seeing PDOS for 9/12/20v ?
2021-07-10 8:27 AM
Hello,
Regarding TCPP03-M20, the datasheet is now available on ST.COM.
https://www.st.com/resource/en/datasheet/tcpp03-m20.pdf
This device is tailored for high voltage controls and protections of Dual Role Power, Dual Role Data applications when used with a STM32 controller with built-in USB-C controller such as STM32G0, STM32G4, STM32L5 or STM32U5.
Among other features, TCPP03-M20 integrates the charge pumps for the two integrated Gate Drivers (provider and consumer path), as well as discharge path for VBUS and VCONN. One key benefit is the power consumption during toggling that can be lowered thanks to the low power mode.
Its associated NUCLEO expansion board is the X-NUCLEO-DRP1M1 with example code for Dual Role Power available by Sept'21 in the X-CUBE-TCPP library.
Best regards,
Mohamed