User Activity

Assuming that STM32H7 is configured as a clock slave with IEEE1588v2 (LAN8742A as PHY), can the received/sync'd clock signal be fed into the internal clock tree to produce 32.768MHz clock output? If so, do any signals need to be routed from one ball ...
I am updating STM32G030F6 via the built-in ROM bootloader from another MCU. 2 issues:The i2c ROM bootloader slave address is actually 0x56, not 0x51 as written in AN2606. I discovered this on this ST community thread: https://community.st.com/s/quest...
This post: https://community.intel.com/t5/Intel-Makers/Low-Voltage-Signaling-SD-Cards/td-p/490563 seems to imply that newer SD cards can operate directly at 1.8V with no translation to 3.3V. Can anyone confirm if STM32H743 supports this?If so, does t...
Examples of the information I want for TI's Code Composer Studio and Microchip's MPLAB X are here:http://software-dl.ti.com/ccs/esd/documents/sdto_ccs_source-control.htmlhttps://microchipdeveloper.com/faq:72
Kudos from