Hi all.I am confused about how I am supposed to provide power to the STM32MP257F-DK as it seems I am not providing enough power to the board when connecting the board to my PC via the STLINK/Power connector as the red Power LED is on and the Green LE...
Hi all, having an issue with programming STM32MP257F-DK/SDCard with the Starter package getting to the stage in the attached screenshot then it seems a connection times out with no success notification popup ?
Hi,Is there a guide out there to get a serial terminal set up with the STLinux "Starter" package on the STM32MP257F-DK up and running ? i.e what settings to use to connect, any needed hardware/connections/cables etc ?
Attached is a log file in a zip from STM32CubeProgrammer with Verbose set to 3. Also there is now no Timeout Error being shown but flashing is stuck at 100% progress with no error messages and there is a Blue led lit on the board.
Searching on this forum shows there is an issue with the B‑LCDAD‑HDMI1 in that for some boards it does not mechanically mate with the host board making the connection very delicate, is this the case with the STM32MP257F-EV1 ?