Hello,I use STMCube IDE v1.3.0 Build: 5720_20200220_1053 (UTC)When building, the include path are not updated with the include path properties.I notice this mis-alignement is caused in the cproject :include path are correct here : <option IS_B...
I found the problem.I don't why but one of my folder had a different configuration than the project.To fix this, I right click on the folder with the problem, then select Ressources configuration then click Reset to default.@Cartu38 OpenDev Thank yo...
Indeed there is something odd with the folderInfo xml tag.It is like I have a folder which is not part of the project and have a different configuration.How can I align this folder with all the project ?
Thank you for your answer, but this is not the case. When building what I can see in the log, the include path are not what I set in the property window of STMCubeIDE. (Under Properties -> C/C++ Build -> settings -> Tool Setting tab -> MCU GCC compil...