User Activity

Hi, I have set the timer4 in center alligned mode 3 and I want to trigger ADC on counter overflow. If I understand correctly the ADC trigger input TIM4_TRGO can be set in timer configuration as update event output but that means also in underflow wil...
hi, P-NUCLEO-IHM001 is marked as obsolete, exist any new successor for motor control hardware? Your Sincerely,Nikos
Hi, I use the timer3 to detect PWM Duty cycle from the input signal. The signal is an angle sensor from a BLDC Motor. That means 0% DCy is 0 grad and 100% is 2pi grad. The sensor has 4096 bit resolution. But I have a problem to detect an overflow int...
Hi, I cannot understand why the TIM8 has in TI1 the label CC4I and the general purpose timer has at TI1 the label CC1I as you can see on the following pictures. And also I want to ask what is the different between TIM8 and TIM1 as advanced control ti...
If the Elf file (executable) has been modified, CubeMonitor does not recognize the changes like STM Studio and the user has to open every single variable node and click on edit exe config node. After this, the addresses has been updated. This is very...
Kudos from