User Activity

HI, please help to check the following build error.I used CubeMX and IAR build tool and the following code.en.stm32cubewl-v1-3-0\STM32Cube_FW_WL_V1.3.0\Projects\NUCLEO-WL55JC\Applications\LoRaWAN\LoRaWAN_End_Node Error is as below,Error[Li005]: no de...
Hello,I wonder whether the size of hex file is over (has problem) or not,please help to let me know it with detailed information,when checking the size of hex file of my code, the size is 12 k bytes like picture,and when checking the datasheet of stm...
Hi,I have one issue in the usage of download function with STM8L051F3,it is sometimes failed, and it made "protection error" with IAR embedded Workbench IDE,I update my schematic, please help to check it,thanks.
Hi, I have some trouble to handle ADS7953 with HAL_SPI_TransmitReceive_DMA api,if using HAL_SPI_TransmitReceive api, it takes long time and impact other operations,so I hope to reduce the communication time with HAL_SPI_TransmitReceive_DMA in the com...
Hi, I would like to know the method to use HAL_SPI_TransmitReceive_DMA API,if providing the example, please help to let me get it through the following email,thankful for your support in advance,email : foodlove1004@naver.comthanks.issue is,if using ...