Posted on June 09, 2018 at 00:54Hello,when I try to open the example with cube to generate code this message appearBut download doesn't work because the current version 12 is not RC1.regards
Posted on June 17, 2018 at 05:47We buy very often from digikey so this would be my first choice, but the digikey support couldn't tell me when I can get one from them
Posted on June 16, 2018 at 15:14sorry for posting in your topic,but the h743 nucleo is still difficult to get on some vendors, is there any reason behind it ?
Posted on June 13, 2018 at 03:38thanks,the tutorial works great, and I got it running with.I'm a bit confused about the U(s)art, does the stm32 communicate with the bluetooth module X-NUCLEO-IDB04A1 and X-NUCLEO-IDB05A1 with uart ? From the shematic...
Posted on June 13, 2018 at 03:26Hello,it's in every ioc from the new package BlueNRG-MSBlueNRG-MS\1.0.0\Projects\STM32L476RG-Nucleo\Applications\ I guess these examples should work or are they just templates for cubemx ?regards
Posted on June 09, 2018 at 04:05I think a workaround is to delete the rc1 in the ioc file with any editor.But then CubeMX doesn't include the Hal Librarys and cmsis (folders are empty).after adding files by hand true studio give me the message, bec...