User Activity

Posted on June 11, 2018 at 20:22Hi,In the Advanced Parameters of the ETH configuration, there is only the LAN8742A external PHY configuration. Is it possible to use an other external PHY (like 8720A) using CubeMX?I tried with the user PHY, but I don...
Posted on May 22, 2018 at 21:29Hi,Is there a way to generate a condition inside the initialization code generated by CubeMx in TrueSTUDIO?I want to do something like this inside the MX_SPI2_Init() :    if (HAL_GPIO_ReadPin(GPIOI, GPIO_PIN_11) == GPI...