User Activity

I have a B-U585I-IOT02A Discovery board, which is connected it to an external ST LSM6DS3 accelerometer via the SPI1 pins on the arduino connector. The issue is that the SCK line is going low when not active even though I have it configured to be hig...
When I generate the code for a simple STM32U5x project with a USART configured and GPDMA configure for the USART TX and/or RX, the initialization code in MX_GPDMA1_Init() will be properly generated if I have my project to generate all the initializat...
Kudos from