i am not able to run any code on bank2 with STM32L151RE with 512kB FLASH.program was loaded on both regions 0x0800 0000 and 0x8004 0000if nBFB2 is checked the code runs ok, if i just unched the code does not run....what am i doing wrong?
if the two are absolute the same, why do you have both? i dont belive that, there must have some differente.... to star with, in the product selector it says 151 have dual boot and 152 not.
i am having problems with dual bank too, i was not able to get it to work...nothing seems to work as expected, but i think the bit nBFB2 should have some affect, if not, how would you build a firmware that needs more then 256k of flash, because above...
it is my first time using dual boot, i am new to STM32 mcu too.i have seen that some MCU need to enable dual boot mode, in STM32L151RE it is naturaly enabled, it was born with dual bank?in the aplication note AN2606 it says "If Value @0x08040000 is w...