User Activity

Hello,we designed a PCB with an ST25R2916B which should connected via I2C.As basis for our design we use the schematic for the X-Nucleo-NFC06A1.Our Problem:If we connect the modified (UM2616, Chap. 3.5.1) X-Nucleo-NFC06A1 to a Nucleo32 running the NF...
Hello,I try to get a feeling for the possible features and use cases of the ST25R3916 NFC Reader chip.One point which sounds very interresting is the capacitive measurement.Are there any code examples (as the linux driver for the ST25R3916) available...
Hi,I try to bring up the NFC06A1 on an Arduino Uno with the Arduino IDE.If I compile the ST example (X_NUCLEO_NFC06A1_HelloWorld), I get an fatal error:C:#######\Documents\Arduino\libraries\STM32duino_ST25R3916\src/rfal_rfst25r3916.h:51:10: fatal err...
Hello Community,I am new in the topic of nfc and programming of nucleo boards.So, the questions can seem to be very stubid ;)For a project I try to bring up a X-Nucleo-NFC06A1 on top of a Nucleo -F446RE.On web (ST,...) I found code examples for diffe...