User Activity

I am working on SensorTile Wireless Industrial Node to ST Dashboard. I am using the software from en.fp-ind-predmnt1_v2.4.0. I have added the device in the dashboard and updated the device certificates and keys. The terminal attempts to establish MQT...
The current script in BlueSTSDK examples (https://github.com/STMicroelectronics/BlueSTSDK_Python) needs to be run as root to scan for bluetooth devices in the vicinity. Question is if it is possible to connect to a bluetooth device and receive data w...
Hardware: SensorTile.boxThe project readme.txt file suggests that the software should start from the memory address 0x08004000 in FLASH. How can I change this when I am downloading the software from the Android app? The board has to be restarted aft...
I am trying to get values at highest data rate(6.6kHz) from Accelerometer on Serial terminal from SensorTile.box. Sensor - LSM6DSOX Binary - 'DataLogExtended.bin' from FP-SNS-STBOX.I tried using the (void)BSP_MOTION_SENSOR_SetOutputDataRate(AccInstan...
I am trying to use DataLogExtended application available with FP-SNS-STBOX1 for SensorTile.box. Apparently, the project works only with a specific version of Unicleo GUI (1.11.0).However, I am unable to download older version of the GUI from ST websi...