User Activity

I recently purchased an L4R9 Discovery board with an MB1314 round LCD.Under STM32Cube_FW_I.4_V1.17.2 / Projects / 32L4R9Discovery / Examples / DSI / DSI_CmdMode_SingleBuffer, there is a reference to a 24bpp frame buffer. The comment cryptically state...
Fresh install (yesterday and today) of CubeIDE 1.7.0 and TouchGFX Designer 4.18.0.In Designer - create a new project, one screen/one control, target is STM32F469I Discovery board.Generates code fine - simulates fine - sends to actual Disco board and ...
When I attempt to create a new project with TouchGFX Designer 4.18.0 using the STM32F469I Discovery as a board setup, the Create button gets to 88% and then consistently fails with the message "Error: Cannot create a file when that file already exist...