User Activity

Hello!  We are a bit stumped here.  We have a product that we are testing at 65C and it seems that the bluetooth connection keeps dropping at this temperature (Connection timeouts).  We are running from a 32K LSE and 32M HSE crystals.  All our parts ...
I have been trying to implement a HCI only interface (LL only set) and pass commands to my board (STM32WB55 Nucleo board - BTStack is the bluetooth stack).  Everything works except for the following sequence-> Connect, pair and bond with Just works (...
I am trying to implement an HCI interface and the stack is reporting almost nothing supported in the HCI_READ_LOCAL_SUPPORTED_FEATURES command. Why is this? Is there a way to enable the features? I am using stack v1.16. I have tried multiple variatio...
So, when I first connect to my USB implementation and send the first 3 bytes to the command/control interface I get 3 zeros. It is not what I sent and interestingly enough I do get the bytes I sent the first time on the next 3 bytes. I have no idea...
Ive seen this issue in various different forms over the last 2 years and it seems like CPU2 is corrupting the TL_RefTable structure while configuring advertising. We are using v1.15.0 of the stack on a STM32WB55. This happens every few hours in the f...
Kudos from