cancel
Showing results for 
Search instead for 
Did you mean: 

STCS1PUR went flashing after connected to power. Need a solution.

TSu.1
Associate III

I am using the same schematics as the datasheet's typical application schematics sugguests. The EN and PWM pin were tied together with Vin. When I connect it to 12V power, It went steady for a couple of seconds then it starts to flash, it turns off and on periodically. so I removed the drain capacitor and connect it across the LED string to Vin (as another question post discussed), it did not solve the issue. What is causing this flash?

This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0