User Activity

Hello,Am using STM32H745XI device same as the disco board and external flash on QSPI (MT25QL512A) single chip flash. IAR IDE is used for development. Though there are reference driver codes available for MT25QL512A but different controller is used. I...
Hello,I wanted to add bluetooth capability to a board with STM32H745 controller. I have a USB port on the board on which I plan to connect a USB bluetooth dongle for bluetooth connectivity.Are there any Development boards and example codes available ...
Hello,Does ST mirco provide a readmade Touchscreen HMI solution which can be interfaced with an existing system and display inputs received through the exisiting system on the display with minimum modifications, should be easily configurable and adap...
Hello,I am using STM32H745 controller with TouchGFX. I wanted to achieve slide transitions such as top to bottom, left to right and right to left for going to other screens. When I slide from top edge to down, slide from right edge to left, slide fro...
Hello,I plan to use STM32H745 controller with touchGFX for UI. Additionally need WIFI capability. What options are available if WIFI is to be used with STM32H745? I dont want to invest time in developing a communication protocol to communicate with a...
Kudos from