User Activity

In memory view, if I have the format set to anything but a column size of 1, is there a way to flip the bytes so they appear in human-readable format?e.g. if I have a uint32_t counter with value 0x12345678, and look at it in memory window, with the v...
Is there a way to split the XPSR register view up so you can see each status bit by its name rather than the 32-bit value?The SFRs have this feature, why do the general registers not have it enabled by default?
Posted on November 11, 2017 at 00:52Hi all,I'm trying to download stm32cube_fw_f4_v1170.zip using the new Libraries manager. I must have tried at least ten times downloading this 418.0 MByte file, it downloads 418.1 MBytes then throws up an error:Er...
Kudos given to