cancel
Showing results for 
Search instead for 
Did you mean: 

X-LINUX-AI-CV OpenSTLinux image to flash on STM32MP157C-DK2

koan
Associate III

Hello,

I'd like to test your X-LINUX-AI-CV OpenSTLinux image on my STM32MP157C-DK2 Discovery kit as explained in the following page

https://wiki.st.com/stm32mpu/wiki/X-LINUX-AI-CV_OpenSTLinux_expansion_package

Do you provide a ready to flash and use X-LINUX-AI-CV OpenSTLinux image somewhere or one have to rebuild it from scratch only?

Thank you

--

Marco

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
Olivier GALLIEN
ST Employee

Hi @koan​ 

No we don't provide ready to flash image.

You have to build it following instruction in wiki page

https://wiki.st.com/stm32mpu/wiki/STM32MP1_artificial_intelligence_expansion_packages

BR,

Olivier

Olivier GALLIEN
In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.

View solution in original post

2 REPLIES 2
Olivier GALLIEN
ST Employee

Hi @koan​ 

No we don't provide ready to flash image.

You have to build it following instruction in wiki page

https://wiki.st.com/stm32mpu/wiki/STM32MP1_artificial_intelligence_expansion_packages

BR,

Olivier

Olivier GALLIEN
In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
koan
Associate III

In fact I had to build it from the beginning. Thanks.