Posted on March 16, 2018 at 09:07I generated a project with cube mx version 4.25 and I have the attached error inKeil Microvision 5.The project is a simple example of STM32f091 (all default)I get the same error in all the projectsThanks for help
Posted on January 11, 2018 at 09:11Hi, I have a micro STM32F011F4 and I try to write in EEPROM via SWD but cube programmer shows an error message (also from CLI) how can I write in EEPROM? (STM32 STlink utility works well) Thank youMarco
Posted on March 21, 2018 at 08:44 Thanks Majerle.Tilen, DFP drivers are installed but every time I edit a project on cube mx I have to redo the procedure of selecting the micro asyou advises (not automatically). I have uninstalled and reinstalled...