User Activity

Posted on October 24, 2017 at 16:00We are planning to use STM32F373RBT6 for the replacement of ATMEL XMEGA_128:I have the following queries related to the design as per my understandings: Is USB2.0 will support device mode only and will be used to ...
Posted on September 29, 2017 at 07:05Please share the equivalent STM32 ultra low power MCU for the below requirement: Flash Memory size [KB] 128 SRAM size [KB] 8 Speed [MHz] 32 DMA controller Yes Communication Peripherals [UART, SPI,I2C]:3 - UART, ...