User Activity

Quick Question.... The Docs say the STM32F767VGT6  has 166 5 V tolerant I/O's I need to put 5V pullups on some of my OUTPUT I/O  !Is the tolerance just for INPUTING ?orWill the Low transistion with a 5V pullup   say   1K   be ok !  
I am working with the L051 chip and having issues with the CubeProgrammer Download..History:   we work with many of the STM32 chips.....and have for years, so well versed in this ...so this is an issue that we have not seen using any of the Tools... ...
I thought the BOOT Modes used BOOT0 & BOOT1(PB2) pinsand to pull BOOT0 (high) and BOOT1(low) to get BOOT MODE (SYSTEM MEMORY) and allow the STM32CUDE programmer!I've looked thru the STM32F723 Docs and PB2 does not seem to show/sharethe BOOT1 pin func...