User Activity

Dear all, I'm working on a project based on stm32h735g-dk I'm using the three ADC in differencial mode. For the ADC 2 I assigned the pin PF13 and PF14 . I'm also using the LCD with touchgfx.I discovered that the pin PF14 even if this is not declared...
Dear All,I'm developing a data acquisition system using a STM32H735G-DK. I'm using Cube IDE and a project generated with CubeMX. I also use touchGFX for the diplay user interface.I managed to do all the acquisition and post ptocessing part on the MCU...