User Activity

Hello,Is there a way to synchronize 2 timers in PWM input so that the second timer will do the PWM input reading in sync (in phase) with the first (master) one ? I see that it is possible with PWM output but for PWM input the "trigger source" is gray...
Dear Community,I looking for some help - I need to be able to read a gamepad controller (in this case logitech wireless F710) with a H723ZG board.  I tried to adapt the mouse and keyboard examples without any success.With the HID_standalone example, ...
Where can I buy additional 34-pin STMod+ cables and DIL socket boards as the ones for STEVAL-STWINBX1 ?See attached picture for the additional parts I'm looking for - can also be used with the PROTEUS1 board but not supplied by default :frowning_face...
Hello, I cannot make the LIS2DU12 working in the Sensor.Tile module. I followed the instruction in the AN5648 but I get random values for X, Y, Z. At first, I'm trying to get the readings in normal continuous mode without FIFO. I can connect the devi...
I cannot find the logic in the schematics about the mapping of the 2 stmod+ connectors.Which pins of the stmod+ correspond to the MCU pins ?Page 7 of the schematic folio is very confusing.I just found pin 3 & 4 of the stmod+2 to be mapped to PG10 & P...