Skip to main content
MBax.2
Associate III
January 27, 2022
Question

How to fix undefined references to secure engine functions in a user application that uses SBSFU

  • January 27, 2022
  • 2 replies
  • 904 views

I have an undefined reference error to several secure engine functions, for example SE_APP_GetActiveFwState

I have read this thread:

https://community.st.com/s/question/0D53W000017PGUKSA4/how-to-call-secureengine-functions-from-my-application

And what I think needs to be done to resolve this problem is to:

-add the function names to se_interface.txt in the SBSFU folder

-rebuild SBSFU

-add the generated se_interface_app.o as additional object file in my project settings > MCU GCC Linker > Misc

-Add other flags, in project settings > MCU GCC Linker > Misc to be the same as the userapp

After doing this however the problem still persists, and I'm having a hard time finding it. I made sure to copy all project settings from the SBSFU UserApp example, added all the includes and compared the linker scripts, now I have reached a dead end...

The contents of my se_interface.txt file is:

SE_APP_GetActiveFwInfo

SE_APP_GetActiveFwState

SE_APP_ValidateFw

This topic has been closed for replies.

2 replies

MBax.2
MBax.2Author
Associate III
January 28, 2022

Found the problem, needed to add defines for ENABLE_IMAGE_STATE_HANDLING not only in my user app, but also in SECoreBin and SBSFU

MBax.2
MBax.2Author
Associate III
January 28, 2022

Now the problem is back for some reason. To make sure it is not in my own app, I took the SBSFU UserApp example and added defines for ENABLE_IMAGE_STATE_HANDLING to SBSFU, SECoreBin and the user app itself.

So the only change I made was to add those defines, and then building fails undefined reference to

SE_APP_ValidateFw and SE_APP_GetActiveFwState.

This is poorly documented in the manuals. Some help would be greatly appreciated. The UserApp example also contains two instances of se_interface.txt both with different content. This is confusing and I do not know what to do with those. The paths for these are:

C:\STM32CubeExpansion_SBSFU_V2.6.0\Projects\B-L475E-IOT01A\Applications\2_Images\2_Images_SBSFU\MDK-ARM\B-L475E-IOT01_2_Images_SBSFU\se_interface.txt

C:\STM32CubeExpansion_SBSFU_V2.6.0\Projects\B-L475E-IOT01A\Applications\2_Images\2_Images_SBSFU\STM32CubeIDE\se_interface.txt