Posted on September 03, 2017 at 14:38
Hello,
I use HAl_Flash driver on STM32L152RBT6 to read, write and erase internal flash memory(EEPROM).
when i try to write new data to flash, thatbitwise OR with previous value.
(
E.g. at address 0...
Posted on July 21, 2017 at 12:02i have stm32l152c- discovery board. i connected the +5v pin to the ground pin and now it seems work on very low power mode and ld1 not lit up and ld2 , ld3 and ld4 lit up very weak. pc not recognize the board. what ca...
Posted on September 03, 2017 at 17:02Thanks to reply.Also HAL_FLASHEx_DATAEEPROM_Erase() not erase anything. Just can erase full page but not a word or a byte.