cancel
Showing results for 
Search instead for 
Did you mean: 

I connected the +5v pin to the ground pin by mistake

mafix mafix
Associate II
Posted on July 21, 2017 at 12:02

i have stm32l152c- discovery board. i connected the 

+5v pin to the ground pin and now it seems work on very low power mode and ld1 not lit up and ld2 , ld3 and ld4 lit up very weak. pc not recognize the board. what can i do?

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
Posted on July 24, 2017 at 15:44

.Hi again

By my mistake  i gave you wrong information   about  152 NUCLEO i have in my desk and Not for discovery board!!

In discovery case  I just checked the schematic  and the most posible is to have malfuction is the D1 diode.

Sorry  for the dissruption!

.

View solution in original post

5 REPLIES 5
Posted on July 22, 2017 at 17:12

Hello

Check your PC usb ports if work normaly.

Remove JP5 and see if your  computer recognizes the stlink

If not,  check D2 shotky diode

In case is not working (D2) you did not just touch the +5v pin to ground.

replace it  (can use temporarily an ordinary silicon diode) and see if the stlink works.

regards

vf

Posted on July 22, 2017 at 17:21

I forgot to write that you have also the option to feed the board from VIN  pin. Read the manual about the voltage you must provide.

Posted on July 24, 2017 at 15:18

hi, thank you for answering me back.

where is JP5? i cant find it even in datasheet. 

Posted on July 24, 2017 at 15:44

.Hi again

By my mistake  i gave you wrong information   about  152 NUCLEO i have in my desk and Not for discovery board!!

In discovery case  I just checked the schematic  and the most posible is to have malfuction is the D1 diode.

Sorry  for the dissruption!

.

Posted on July 24, 2017 at 23:59

thanks bro, i got problem is circuit protection when you mentioned D2!

i replaced D1 and the board is healthy now!:D