User Activity

Hello ST team. i wrote about L9369's AD measurement before, but i can't get any response from ST team.(my question is : https://community.st.com/t5/interface-and-connectivity-ics/l9369-getting-voltage-from-sh1-sh2/td-p/589290)i also can't find any me...
Hello. ST team.i'm using L9369's voltage measurement function.i read L9369 manual, and i send below SPI commands(no.0~6) for initial driving.(my purpose is to drive FET : HS1 A, B ON / LS2 A,B ON)00xb5019ff810xb5a15fef20xb720b54d30xb480aa9840x40a0000...
Hello. I'm using L9369 IC and have a problem.   Stage A is not working.   i made control code for Stage A,B. (they are very similar)   i used below two command for H-brdige operation.   but. current was not flow.   here is phenomenon. 1.Low side GL1,...
Hello. i'm using L9369 and i have a question about it.According to the datasheet i have, L9369 has 4 channel CSA(what is the full name of CSA?) and below picture is the example of pin definition. and there are registers that have Current sensing func...
Hello. I'm Using L9369 for H-bridge control.I'm trying to set GIO0~8 pin high(Button interface), but i can't(Analog Output - SPI control)i'm using SPI command, and i saw L9369's manual and i follow the instruction below steps to set GIOx pin as high....
Kudos from