cancel
Showing results for 
Search instead for 
Did you mean: 

STM32L412 : Could we used the SPI interface control the 5V LED Driver IC.

HungKai.Chien
Associate III

Could we used the SPI interface control the 5V LED Driver IC?

  1. STM32L412's VCC is 3.3V, SPI's pins are FT_f type.
  2. LED Driver IC's VCC is 5V.

Is there anything that needs extra attention?

Will there be problems with SPI operation?

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
TDK
Super User

It should work, provided pins are correctly configured.

You need to ensure +5V is never applied when the chip is not powered (VDD=0).

What LED driver? Make sure that 3.3V is guaranteed to be logic high.

If you feel a post has answered your question, please click "Accept as Solution".

View solution in original post

4 REPLIES 4
TDK
Super User

It should work, provided pins are correctly configured.

You need to ensure +5V is never applied when the chip is not powered (VDD=0).

What LED driver? Make sure that 3.3V is guaranteed to be logic high.

If you feel a post has answered your question, please click "Accept as Solution".

Hi TDK,

Thanks a lot.

The LED Driver is IS31FL3743B.

The Vih min is 2.4V.​

Hi TDK,

About this question, does ST have any document for SPI operation @ 5V?

I don't think you'll find anything that specific. What are you looking to find out? The reference manual is typically the best source of information, followed by the datasheet for chip-specific things.

The SPI would be operating at the STM32's voltage, which is (typically) 3.3V. Only the MISO line would be 5V.

If you feel a post has answered your question, please click "Accept as Solution".