User Activity

Hey,I note That There is an instruction ERROR in en.x-cube-spn3 code.in Powerstep01_SetDeviceParamsToGivenValues(uint8_t deviceId, powerstep01_Init_u_t *initPrm); function of powerstep01.c file, at line 1912 to 1914, the instruction, " Powerstep01_Cm...
Hey,i bought <nucleo-F401RE> and <x-NUCLEO-IHM03A1> boards in order to drive the NEMA 17 "QSH-4218-51" bipolar step motor. this one can be supply under 24V with 1A phase current. Using "BASETech-305" Volage Generator, i supplie the <x-NUCLEO-IHM03A1>...
As STM32CubeMX 4.25.1 is not compatible with <X-CUBE-SPN14> Stepper motor driver software expansion for STM32Cube package, i tried to include manualy the Driver to my project. Then, i copy the <BSP> repertory from <en.x-cube-spn14\...\Drivers> to my ...
Posted on May 24, 2018 at 12:53Hey,I am getting started with FreeRTOS on NUCLEO-FO72RB.i set UART communication using DMA.i would like to writre tu UART from muliple taske using queue with size of 16 items;so i created 3 tasks.- one task1 to receive...
Posted on January 09, 2018 at 11:55Hi, I have on module SPWF01SA that return '+WIND:11:Initial SPI read failed: 00000000' on power ON.what does it mean? how can#wifi-spwf01sa #spwf01sa
Kudos from