C1257
Associate
since
2020-07-15
2023-06-14
User statistics
2
Posts
0
Solutions
0
Kudos given
0
Kudos received
STMicroelectronics Community
About C1257
Options
Report User
User Activity
Posts
Replies
I am using STM32CubeIDE for STM32 discovery board. But when I try to connect the board, it gives error and not able to connect to the board.
2020-09-04
Error in final launch sequence:Failed to start GDB serverFailed to start GDB serverError in initializing ST-LINK device.Reason: (6) ST-L
I have to interface the following in my application: Ethernet – 1 no. SD memory card – 1 no. IOs 24 UART (Serial) – 1 no. LCD – 1 no. And microcontroller selected is STM32F429ZIT6. Please suggest the evaluation board.
2020-07-15
No replies to display.