User Activity

Good day! I have some problems with UDP packets transmission. Seems that UDP packets sometimes not sent Board was developed on STM32F407VET6 using LAN8742A driver. UDP packets with size 1200 bytes are sending using timer 10 in 200 ms interval. void H...
Posted on October 17, 2017 at 15:11We have project generated in STM32CubeMX v.4.21.0 based on STM32F407VETx  MCU. This project use USB_OTG_HS to communicate with host computer. When we write program to flash at origin value ORIGIN = 0x8000000 all wo...