STM32 MPUs Embedded software
STM32 MPUs Solutions
MEMS and sensors
MEMS (sensors)
Imaging (sensors)
Automotive & Transportation
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
GGeno.1
Associate II
since
2022-06-18
2023-06-14
User statistics
5
Posts
0
Solutions
0
Kudos given
0
Kudos received
STMicroelectronics Community
About GGeno.1
Options
Report User
User Activity
Posts
Replies
I have a problem with GDB debugger on stm32F401re, i can't connect to target because it is not found. How can i resolve?
2022-06-18
Re: I have a problem with GDB debugger on stm32F401re, i can't connect to target because it is not found. How can i resolve?
2022-06-19
I have tried but the problem persist.
Re: I have a problem with GDB debugger on stm32F401re, i can't connect to target because it is not found. How can i resolve?
2022-06-19
I have already done upgrade firmware, the problem is happened after a session of debug on the firmware with SYS debug disable in the configuration...could be this the cause?
Re: I have a problem with GDB debugger on stm32F401re, i can't connect to target because it is not found. How can i resolve?
2022-06-19
Thank you for the answer... I have this configuration... there are already under reset and low power debug.
Re: I have a problem with GDB debugger on stm32F401re, i can't connect to target because it is not found. How can i resolve?
2022-06-19
In the directory of mcu i have found the file FAIL.TXT with this message: "The interface firmware FAILED to reset/halt the target MCU"