User Activity

Posted on January 23, 2018 at 14:33Hello,I have been looking for a library for the ds18b20 compatible with stm32f0 and with the HAL driver but without success, so I decided to modify old one to make it compatible.this lib uses while loop delay, the ...
Posted on July 26, 2017 at 13:32Hello,I noticed that the stm32F429 disco does not have the CS43L22 circuit nor a 3.5mm jack for audio output as its rival the F407, but it has two internal DAC output, which can be used to play a wav file.If anyone ha...
Posted on March 07, 2017 at 07:09Helloi have created my project with STM32 CubeMX and everything works like a charm, But i am stuck with the clock, i want to configure a RTC clock with Vbat pin to keep time running even if VDD power loss, apparently...