Wav player using DAC in STM32F429
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2017-07-26 4:32 AM
Hello,
I noticed that the stm32F429 disco does not have the CS43L22 circuit nor a 3.5mm jack for audio output as its rival the F407, but it has two internal DAC output, which can be used to play a wav file.
If anyone has an example compatible with HAL libraries would be very nice !
Farouk
#stm32f429-disco #wav- Labels:
-
STM32F4 Series
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2017-07-26 10:17 AM
While it is not a direct code solution,
offers a detailed instruction on how to implement an audio WAV player from FATFS using the internal DAC and DMA/TIM6. It is toward the end of the document.- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2017-07-28 7:49 AM
Thank you
Pappas.Chris
for your reply,Well after reading this application note, thisexample seemsfor SPL library, and i didn't find this examplein the STM32F1 firmware pack !
I don't understand why this function was not integrated directly into the cubeMX