User Activity

Connected to STM32F411CE I know this post is not fully related to STM32 but I am posting here as this forum is somewhat active so I can get some help. SIMCOM forums are pretty much dead. I am interfacing sim7080 with stm32, but for this test I am bas...
MCU: STM32F411CEU6 So, I am having a weird issue. I created a bootloader for my application to accommodate OTA updates. Bootloader makes decision when it has new firmware inside external flash(the application code tells it), then bootloader loads tha...
MCU : STM32F411CEU6 Hello everyone. I have an application in which I want to get image end address from linker. Here is a full context of what I want to do, I have a struct living in start of my image, which basically tells the bootloader usefull inf...
Hi, I wanted to clock my timer output using LSE crystal, but unfortunately only tim2 is supported with this feature. But then I saw an option of LSCO as output in cubemx, this enables the pin on MCU and according to documentation this output LSE cloc...
Hi, I was trying to install stm cubeide and it says that this software is not available and then I tried others and says the same thing. I am also logged in. I have attached the screenshot.  
Kudos from