Posted on August 28, 2017 at 12:02 Hi, I try to receive characters over USART1 using the StdPeriphLibrary (System Workbench STM32, MCU is SM32F103C8B), but after I get the data the program stuck (transmission works perfectly). The ISR is: v...
Posted on August 31, 2017 at 15:36After I tried to enable Timer which also did not work I thought the code may be right, the problem was with the SystemWorkbench. Then I found that the AC6 makes a default startup file with only some interrupt. Downl...