STM32F103 USART RX interrupt notfires, then stuck
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2017-08-28 3:02 AM
Hi,
I try to receive characters over USART1 using the StdPeriphLibrary (System Workbench STM32, MCU is SM32F103C8B), but after I get the data the program stuck (transmission works perfectly).
The ISR is:
void USART1_IRQHandler(void)
{ uint16_t rx; if(USART_GetITStatus(USART1,USART_IT_RXNE)!=RESET) // check RX interrupt { rx = USART_ReceiveData(USART1); led_toggle(); } }Whenever data arrives the LED should toggle, but nothing happens, just hangs the code.
USART settings:
void
USART1_Init( void ) {/* USART configuration structure for USART1 */
USART_InitTypeDef usart1_init_struct;
/* Bit configuration structure for GPIOA PIN9 and PIN10 */
GPIO_InitTypeDef gpioa_init_struct;
/* Enalbe clock for USART1, AFIO and GPIOA */
RCC_APB2PeriphClockCmd(RCC_APB2Periph_USART1 | RCC_APB2Periph_AFIO |
RCC_APB2Periph_GPIOA, ENABLE);
/* GPIOA PIN9 alternative function Tx */
gpioa_init_struct.GPIO_Pin = GPIO_Pin_9;
gpioa_init_struct.GPIO_Speed = GPIO_Speed_50MHz;
gpioa_init_struct.GPIO_Mode = GPIO_Mode_AF_PP;
GPIO_Init(GPIOA, &gpioa_init_struct);
/* GPIOA PIN9 alternative function Rx */
gpioa_init_struct.GPIO_Pin = GPIO_Pin_10;
gpioa_init_struct.GPIO_Speed = GPIO_Speed_50MHz;
gpioa_init_struct.GPIO_Mode = GPIO_Mode_IN_FLOATING;
GPIO_Init(GPIOA, &gpioa_init_struct);
/* Enable USART1 */
USART_Cmd(USART1, ENABLE);
/* Baud rate 9600, 8-bit data, One stop bit
* No parity, Do both Rx and Tx, No HW flow control
*/
usart1_init_struct.USART_BaudRate = 9600;
usart1_init_struct.USART_WordLength = USART_WordLength_8b;
usart1_init_struct.USART_StopBits = USART_StopBits_1;
usart1_init_struct.USART_Parity = USART_Parity_No ;
usart1_init_struct.USART_Mode = USART_Mode_Rx | USART_Mode_Tx;
usart1_init_struct.USART_HardwareFlowControl = USART_HardwareFlowControl_None;
/* Configure USART1 */
USART_Init(USART1, &usart1_init_struct);
/* Enable RXNE interrupt */
USART_ITConfig(USART1, USART_IT_RXNE, ENABLE);
/* Enable USART1 global interrupt */
NVIC_EnableIRQ(USART1_IRQn);
}(the original code is from
http://pandafruits.com/stm32_primer/stm32_primer_uart.php
)Polling the RX works well.
Is there any suggestions?
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2017-08-28 3:30 AM
Sorry about the title, of course interrupt DOES fire, then stuck...
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2017-08-31 6:36 AM
After I tried to enable Timer which also did not work I thought the code may be right, the problem was with the SystemWorkbench. Then I found that the AC6 makes a default startup file with only some interrupt. Downloaded CubeMX, made a very simple projec, copied the startup file to the project, and voila!
Everything works!