User Activity

Posted on February 05, 2017 at 15:45HelloI've established that the pins on bottom of Nucleo-F767ZI (144) are ST Zio connector � CN7, CN8, CN9, CN10 (relevant 2 pages from UM are attached).I want to create PCB on top of which I will be able to plug i...
Posted on February 05, 2017 at 10:06Wish List is closed and something came up to my mind. It's a stupid idea, but useful:Would it be possible to include like 2x12 pin header on Nucleo/Disco, with alternate functions configuration, to direct chosen C...
Posted on February 05, 2017 at 09:33Hello farnell has http://uk.farnell.com/rf-solutions/gamma-ard/arduino-shield-868mhz-telemetry/dp/2500109:It's 868MHz Operation Transceiver, link is above.I think there's 5V vs. 3.3V problem, is that correct? Only...
Posted on February 04, 2017 at 16:52I'm using an Arduino protoshield and see how cool thing it is. I think people are mostly skeptical about Arduino support in ST Zio / Nucleo, however the ability to arrange on Arduino protoshield, solder and then p...