User Activity

HI Sir,the switching frequency below input 24V 0.04A output 12Vis that normal. the switching frequency below, input 24V 0.01A output 12Vthe switching frequency below input 24V 0.33A output 12V the circuit see below:  
HI Sir,how do we define the switching frequency of the L7987the switching frequency range is between 250KHz and 1.5MHzlooks like if the switching frequency is set to 1.5MHz, the ripple appears to be much smaller, so can we set it to 1.5MHz under norm...
HI Sir,we have two different results of the ripple noisebase on same PCBA design, but different L7987 origin:1. Mark of "ST e3 G9207,L7987, CHN 3L0",ripple noise 2.2V 2.9KHzinput 24V, output 12V, load 5ohm 2.4A 2. Mark of "ST e3 7B658, L7987, PHL 037...
HI Sir,we have applied L7987 and L7987L on our touch display computer,we don't have enough stock for nowis there any substitued parts availablethanks�?With best regards,PZ​
HI, how can I connect a PTC resistor to STM32G030K6T6, the reference power is from ext. LDO or not, thanks,
Kudos given to