cancel
Showing results for 
Search instead for 
Did you mean: 

L7987 and L7987L substitued parts

PZha.1
Associate III

HI Sir,

we have applied L7987 and L7987L on our touch display computer,

we don't have enough stock for now

is there any substitued parts available

thanks�?

With best regards,

PZ​

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
Peter BENSCH
ST Employee

The A7987 is functionally identical to the L7987. However, it is more expensive because of the automotive approval, so I did not consider it. If you accept the higher price, you can of course also use the A7987.

Regards

/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

View solution in original post

7 REPLIES 7
Peter BENSCH
ST Employee

The L7987 (3A) and L7987L (2A) can be used up to 61V input voltage and unfortunately do not have an alternative type.

If the problem is solved, please mark this thread as answered by selecting Select as best, as also explained here. This will help other users find that answer faster.

Regards

/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
PZha.1
Associate III

Hi Sir,

can we use A7987 as alternative.

thanks!

PZ

Peter BENSCH
ST Employee

The A7987 is functionally identical to the L7987. However, it is more expensive because of the automotive approval, so I did not consider it. If you accept the higher price, you can of course also use the A7987.

Regards

/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

HI Peter,

thanks for your conformation.

with best regards,

PZ

Peter BENSCH
ST Employee

Great!

If the problem is solved, please mark this thread as answered by selecting Select as best, as also explained here. This will help other users find that answer faster.

Good luck!

/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

HI Peter,

could you please advise that how to select the resistors for the voltage setting, 

are the resistor volume same for L7987, L7987L and A7987 voltage setting.

thanks.

with best regards,

PZha

for example: output 5V,

60.4K and 11K,=5.19V

43K and 8.2K =4.99V
6.04K and 1.1K=5.19V
3K and 0.56K=5.08V

which one is more suitable. any difference

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.