User Activity

Posted on April 23, 2018 at 19:14HI there,This isn't a question related to ST products, but I'm just curious about something that I started noticing. I am developing my project on Atollic TrueSTUDIO, and when I build the project using the CDT Manged...
Posted on February 07, 2018 at 21:12Hello, I'm just wondering what is the threshold voltage used to determine if an external interrupt due to falling or rising edge should occur. I'm attempting to find it in the datasheet, but unsure at which value ...
Posted on February 25, 2017 at 04:22Hi,I'm using a STM32F303 (landing page: http://www.st.com/en/microcontrollers/stm32f303k8.html) for one of my project. I have PA0 configured as a GPIO output with push pull used to turn ON/OFF a BJT. I also have P...
Posted on January 02, 2017 at 19:16I was wondering if I am able to connect an external voltage reference of 4.096 volts to VDDA (to be used as a voltage reference for ADC) without damaging the board?
Posted on December 29, 2016 at 19:44Hi, I have a NUCLEO-F303 board which I would like to use to communicate to two devices using SPI. The NUCLEO would be sending and receiving data to and from the devices via MOSI and MISO.Looking through the datash...