cancel
Showing results for 
Search instead for 
Did you mean: 

External VRef on VDDA on NUCLEO-F303K8

William Huang
Associate II
Posted on January 02, 2017 at 19:16

I was wondering if I am able to connect an external voltage reference of 4.096 volts to VDDA (to be used as a voltage reference for ADC) without damaging the board?

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
Khouloud GARSI
ST Employee
Posted on January 03, 2017 at 10:42

Hello William,

You should respect the values indicated on the STM32F303x8 reference manual and datasheet:

                                                  2 V ≤ VDDA = VREF+ ≤ 3.6 V

If this answers your request, please click on correct 

:)

.

Khouloud.

View solution in original post

2 REPLIES 2
Khouloud GARSI
ST Employee
Posted on January 03, 2017 at 10:42

Hello William,

You should respect the values indicated on the STM32F303x8 reference manual and datasheet:

                                                  2 V ≤ VDDA = VREF+ ≤ 3.6 V

If this answers your request, please click on correct 

:)

.

Khouloud.

Posted on January 03, 2017 at 10:43

Doesn't that exceed device maximums? Review part data sheet.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..