Posted on April 05, 2013 at 23:37For regulator on and internal reset off should the pdr_on be connected to vcc or vdd or left floating? Thanks #stm32f417-ufbga176
Posted on August 01, 2013 at 03:30The stm32f4xx_tim.h file states that the TIM_TimeBaseInitTypeDef structure is used with all TIMx except for TIM6 and TIM7. Is this part of the problem? Which structure definition is used for TIM6 and TIM7?