Posted on November 09, 2017 at 17:06 Hi, I'm wondering why a different macro definition is used for the stm32f0xx_hal_pcd.h header file of the USB HAL driver than the other HAL drivers. Macro definition of multiple C statements shall be placed wi...
Posted on December 23, 2016 at 11:27 The original post was too long to process during our migration. Please click on the provided URL to read the original post. https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&id...
Posted on December 23, 2016 at 11:25Hi,Yes, this is feasible. Here is attached a source code snippet which I used before to generate that waveform.Which is of interest in that snippet is the void commutate5(uint32_t); function's body. it describes t...
Posted on July 09, 2013 at 19:10I think that we all have the same feeling regarding the quality of documentation. But, it is also fair to mention that a remarkable enhancement is observed over the whole documentation.From my point of view microcontr...
Posted on April 05, 2013 at 21:14Hello,You may refer to the PIL MMS-MIC/12/7477 document published on ST web-site. It mentions clearly that LSE’s transconductance was decreased in rev X die compared to rev Y die.I think this is most probably the rea...
Posted on February 22, 2013 at 12:36Hi,If we take an oversight of the STM32 MCUs documentation, u will see that the coarse calibration was first introduced by STM32F1 MCUs family. STM32F2 MCUs’ RTC is also built-in with coarse calibration. But for r...