Posted on January 31, 2013 at 13:38
Hi,
I have a problem for the second time, I don't know why but hardware breakpoint, sometimes, still in stm and I can't delete it.
I use OpenOCD 0.6.1 and gdb
This is my gdb log :
...
Posted on January 24, 2013 at 12:14
Hello,
I try to get a ssb1322 oled display working with a stm32f4 board.
The display is NHD-2.8-25664UCY2 from new heaven. The recurrent problem with this display is power, so I power it with a...
Posted on February 01, 2013 at 00:30
I have checked my openOCD.cfg, it is ok. It may be a gdb bug.
I have fix the problem, I don't know how. Many hours of search... And it finally come back to life.
Now I have my 6 breakpoints an...
Posted on January 31, 2013 at 21:57
No one can help me ?
I have moved the fonction elsewhere and It was resolv the problem for a moment but, now I have 2 hardware breakpoint in the sky with diamond, look at log :
(gdb) target ...
Posted on January 28, 2013 at 10:44It works ! But only in software SPI for instance. I don't know the original probleme, may be several things, I do lot of modifications since my last software SPI test. As I say, I am not an electronician, but I thi...
Posted on January 27, 2013 at 12:33Don't be glad, I am not an electronician. I have not used an oscilloscope since school, 15yr ago ^^ I have set the clock to 281khz for testing. I do many test, many different timing, I hope the rest of my project ...
Posted on January 25, 2013 at 21:38In fact, I can see SCK pulses at 125ns/div. The result is crapy but coherent. I will look for a better oscilloscope if I want to check pin synchronisation.. I have tried with a software spi on same pins, the result...